REC.OFF

Description

REC.OFF turns the recorder off. In order to set the recorder again, the recorder must first be armed and then a trigger set.

General Information

Type

R/W Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.ACTIVE, REC.DONE

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Related Topics

Scope

REC.READY