REC.STOPTYPE

Description

This parameter sets the stop type for the recording.

0 = Recorder fills in the buffer once.

1 = Recorder runs, continuously filling the recording circular buffer.

To stop RT recording, execute REC.OFF.

General Information

Type

R/W Parameter

Units

N/A

Range

0 or 1

Default Value

0

Data Type

Integer

See Also

REC.RETRIEVEDATA, REC.RETRIEVESIZE

Start Version

M_01-00-00-000

Related Topics

Scope