REC.TRIG

Description

REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.

REC.TRIG sets the value of REC.DONE to 0.

After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.

No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.RETRIEVE, REC.OFF

Start Version

M_01-00-00-000

*For Profinet, write a value of 0 into the PNU to execute a command.

Related Topics

Scope