REC.TRIGMASK

Description

The keyword REC.TRIGMASK is only active when the trigger type (REC.TRIGTYPE) for the recorder is set to 5, which means "Bit Mask Parameter". The trigger is executed once the trigger level (REC.TRGIVAL) matches the data of the trigger parameter (REG.TRIGPARAM) bitwise mask with REC.TIRGMASK.

General Information

Type

Read / Write

Units

N/A

Range

0 to 2^63-1

Default Value

0

Data Type

Integer

See Also

REC.TRIG
REC.TRIGPARAM
REC.TRIGVAL
REC.TRIGSLOPE
REC.TRIGPO

Start Version

M_01-00-00-000