REC.TRIGPARAM

Description

REC.TRIGPARAM sets the parameter on which the recorder triggers.

This parameter is only used when REC.TRIGTYPE = 2.

Input values are:

  1. One of the set drive parameters list that can be set as a trigger. The available parameters for trigger are: PL.ERR , PL.CMD, PL.FB, VL.CMD, VL.FB, ILClosed"Instruction list" This is a low-level language and resembles assembly.CMD, and IL.FB.
  2. Internal value or variable of the drive (same as for DRV.MEMADDR input).

General Information

Type

R/W Parameter

Units

N/A

Range

N/A

Default Value

IL.FB

Data Type

String

See Also

REC.TRIG

Start Version

M_01-00-00-000

Related Topics

Scope