REGEN.REXT
Description
REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.
General Information
|
Type |
NV Parameter |
|
Units |
Ω |
|
Range |
0 to 255 Ω |
|
Default Value |
0 Ω |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
35C2h/0 |
M_01-00-00-000 |
Related Topics