REGEN.WATTEXT
Description
Sets the regen resistor's power fault level for an external regen resistor (when REGEN.TYPE = -1).
Above this fault level, the regen resistor's PWM wil be 0 and a fault will be issued.
General Information
|
Type |
R/W parameter |
|
Units |
W |
|
Range |
0 to 62,000 W |
|
Default Value |
1000 W |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3414h/0 |
M_01-00-00-000 |
Related Topics