TEMP.CONTROL

Description

Reads the temperature of the control board temperature sensorClosedA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.

General Information

Type

R/O Parameter

Units

Degrees Celsius

Range

-127 to 128

Default Value

N/A

Data Type

Integer

Start Version

M_01-09-00-000

Related Topics

DRV.TEMPERATURES | TEMP.POWER1 to TEMP.POWER3