USER.INT1 to USER.INT24

Description

This parameter stores an integer value. To retain this value after a power-cycle, a "Save to Device" command must be performed from the Parameter Load/Save view in WorkBench.

General Information

Type

R/W Parameter

Units

N/A

Range

-2,147,483,648 to 2,147,483,647

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000