VBUS.HALFVOLT
Description
This parameter is used to change voltage thresholds to allow -07 drive types to work at an -06 drive type's voltage thresholds. For information on voltage ratings and drive types see AKD Models.
When the VBUS.HALFVOLT value is changed, the revised thresholds take effect immediately.
VBUS.HALFVOLT only affects -07 drives.
| Value | Description |
|---|---|
| 0 | The original voltage thresholds are used for the functions mentioned below. |
| 1 | -07 drives use voltage thresholds of -06 drives. |
This parameter has an impact on the following voltage-thresholds:
- DC-bus over-voltage threshold (see VBUS.OVFTHRESH ).
- The regen-resistor enable/disable voltage thresholds.
- The inrush-relay enable/disable voltage thresholds.
-
-
The DC-bus under voltage fault threshold (see VBUS.UVFTHRESH ) is a user selectable command. It means that the user is responsible for setting the under voltage threshold to a proper value in case that the AKD is supplied with a lower DC-bus voltage than the rated voltage.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-04-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5261h/0 |
M_01-04-01-000 |