VL.FFDELAY
Description
VL.FFDELAY sets the delay applied to the velocity feedforward term that is passed into the velocity loop integrator. The delay is applied to the velocity feedforward, and then subtracted from the current velocity feedforward term. This difference is the value fed into the velocity loop integrator. If tuned correctly, this delay will help reduce position following error and velocity following error.
This filter is considered a feedforward. For best results it should be set in conjunction with PL.PDELAY.
After making an approximation of the Open Loop bandwidth
In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz (Hz) in the Performance Servo Tuner, calculate VL.FFDELAY:
VL.FFDELAY = 1 / (Open Loop BW (Hz) * 2π) * 1,000,000
-
- 1,000,000 = seconds to microseconds
General Information
|
Type |
R/W Parameter |
|
Units |
Microseconds |
|
Range |
0, 100 to 625,000 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-13-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
53D6/0 |
M_01-00-00-000 |
Related Topics