VL.KO
Description
VL.KO is used to scale the observer model to match the load. When VL.KO is tuned properly, VL.MODEL will match VL.FB , except when there is an unspecified offset between the two.
General Information
|
Type |
R/W Parameter |
|
Units |
Internal |
|
Range |
0 to 65,535 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
51B3h/0 |
M_01-00-01-000 |
Related Topics