VL.VFTHRESH

Description

This parameter reports the overall overspeed fault threshold. Whichever of the following thresholds has the smallest value is used as the overall overspeed fault threshold:

  • User overspeed threshold (VL.THRESH).
  • Motor mechanical overspeed threshold (1.2 x MOTOR.VMAX)
  • If MOTOR.TYPE = 6, the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (MOTOR.KE x sqrt(2))).

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Float

Start Version

M_01-10-03-000

Related Topics

Velocity Loop | VL.THRESH | MOTOR.VMAX