WS.DISTMAX
Description
This parameter sets the maximum movement that is allowed for finding commutation. If this value is too small, FF475 , "Wake and Shake. Too much movement", may occur before wake and shake is finished. The bigger this value, the more movement is allowed for wake and shake. This value is application dependent.
General Information
|
Type |
R/W Parameter |
|
Units |
deg (position units) |
|
Range |
0 to 90 deg |
|
Default Value |
15 deg |
|
Data Type |
S64 |
|
See Also |
N/A |
|
Start Version |
M_01-01-00-101, M_01-02-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3494h/2 |
M_01-00-00-000 |
Related Topics