WS.FORCEOFF
Description
Disables the automatic Wake and Shake procedure if the identified feedback type is sine encoder without halls (FB1.IDENTIFIED = 21) and the encoder pitch is equal to the motor pole pitch of the linear motor.
| Value | Description |
|---|---|
| 0 | enabled |
| 1 | disabled |
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-16-02-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
541fh/0 |
M_01-16-02-000 |
Related Topics