ClearCtrlErrors

Clears the active errors and alarms on the controller. Only clearable errors will be cleared. See PDMM and PCMM Errors and Alarms for a list of errors and alarms that may be generated.
Arguments
Input
| EN | Data Type | Enable the function |
Output
| Q | Data Type | BOOL |
-
-
If clearable and non-clearable errors are present and this function is called, the Output Q will be turned to true but the non-clearable errors will remain.
Examples
FBD
FFLD
ST
//Attempt to clear active controller level errors and alarms(such as E33)
IF ClearControllerErrors THEN
ClearCtrlErrors();
END_IF;