LoadString
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Load a string from the active string table.
Inputs
ID: DINT ID of the string as declared in the string table
Outputs
Q : STRING Loaded string or empty string in case of error
Remarks
This function loads a string from the active string table and stores it into a STRING variable. The StringTable() function is used for selecting the active string table.
The "ID" input (the string item identifier) is an identifier such as declared within the string table resource. You don't need to "define" again this identifier. The system does it for you.
ST Language
Q := LoadString (ID);
FBD Language
FFLD Language
IL Language:
See also