SetWithin
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Force a value when inside an interval.
Inputs
IN : ANY Input
MIN : ANY Low limit of the intervalMAX : ANY High limit of the intervalVAL : ANY Value to apply when inside the interval
Outputs
Q : ANY Result
Truth Table
| In | Q |
|---|---|
| IN < MIN | IN |
| IN > MAX | IN |
| MIN < IN < MAX | VAL |
Remarks
The output is forced to VAL when the IN value is within the [MIN ... MAX] interval. It is set to IN when outside the interval.