ArrayToString / ArrayToStringU
Function
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Copy an array of SINT to a STRING.
Inputs
SRC : SINT Source array of SINT small integers (USINT for
ArrayToStringU)
DST : STRING Destination STRING
COUNT : DINT Numbers of characters to be copied
Outputs
Remarks
In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
This function copies the COUNT first elements of the SRC array to the characters of the DST string. The function checks the maximum size of the destination string and adjust the COUNT number if necessary.
ST Language
Q := ArrayToString (SRC, DST, COUNT);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language
Not available
See also