ASCII
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the ASCII code of a character within a string
Inputs
IN : STRING Input string
POS : DINT Position of the
character within the string
(The first valid position is 1)
Outputs
CODE : DINT
ASCII code of the selected character
or 0 if position is invalid
Remarks
In FFLD language, the input rung (EN) enables the operation, and the output
rung keeps the same value as the input rung. In IL
"Instruction list"
This is a low-level language and resembles assembly language, the first parameter
(IN) must be loaded in the current result before calling the function. The other
input is the operand of the function.
ST Language
CODE := ASCII (IN, POS);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO is equal to EN *)
IL Language:
See also