GETSYSINFO
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Returns system information.
Inputs
INFO : DINT Identifier of the requested information
Outputs
Q : DINT Value of the requested information or 0 if error
Remarks
The INFO parameter can be one of the following predefined values:
| Value | Definition |
|---|---|
_SYSINFO_TRIGGER_MICROS |
programmed cycle time in micro-seconds |
_SYSINFO_TRIGGER_MS |
programmed cycle time in milliseconds |
_SYSINFO_CYCLETIME_MICROS |
duration of the previous cycle in micro-seconds |
_SYSINFO_CYCLETIME_MS |
duration of the previous cycle in milliseconds |
_SYSINFO_CYCLEMAX_MICROS |
maximum detected cycle time in micro-seconds |
_SYSINFO_CYCLEMAX_MS |
maximum detected cycle time in milliseconds |
_SYSINFO_CYCLESTAMP_MS |
time stamp of the current cycle in milliseconds (OEM |
_SYSINFO_CYCLEOVERFLOWS |
number of detected cycle time overflows |
_SYSINFO_CYCLECOUNT |
counter of cycles |
_SYSINFO_APPSTAMP |
compiling date stamp of the application |
_SYSINFO_CODECRC |
CRC |
_SYSINFO_DATACRC
|
CRC of the application symbols. |
_SYSINFO_FREEHEAP
|
Available space in memory heap (bytes) |
_SYSINFO_DBSIZE
|
Space used in RAM (bytes) |
_SYSINFO_ELAPSED
|
Seconds elapsed since startup |
_SYSINFO_CHANGE_CYCLE
|
Indicates a cycle just after an On Line Change |
_SYSINFO_WARMSTART
|
Non zero if RETAIN variables were loaded at the last start |
_SYSINFO_NBLOCKED
|
Number of locked variables |
_SYSINFO_NBBREAKPOINTS
|
Number of installed breakpoints |
_SYSINFO_BIGENDIAN
|
Non zero if the runtime |
_SYSINFO_DEMOAPP
|
Non zero if the application was compiled in DEMO mode |
In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL
"Instruction list"
This is a low-level language and resembles assembly, the
input must be loaded in the current result before calling the function.
ST Language
Q := GETSYSINFO (INFO);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)