Programming Languages - Overview
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger application language.
Below are the available programming languages of the IEC
"International Electrotechnical Commission"
IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard:
- Sequential Function Chart (SFC)
- Function Block Diagram (FBD)
- Free Form Ladder Diagram (FFLD)
- Structured Text (ST)
- Instruction List (IL)
You have to select a language for each program or User-Defined Function Block of the application.
-
- Replace with note text When using FFLD or FBD languages, be sure to review Use of ST expressions in graphic language
Refer also to the following pages about the IEC 61131-3 programming languages:
Program organization units
Data types
Structures
Variables
Arrays
Constant expressions
Conditional compiling
Handling exceptions