RIGHT
A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Extract characters of a string on the right.
Inputs
IN : STRING Character string
NBC : DINT Number of characters to extract
Outputs
Q : STRING String containing the last NBC characters of IN.
Remarks
In FFLD language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.
In IL
"Instruction list"
This is a low-level language and resembles assembly, the
first input (the string) must be loaded in the current result before calling the function.
The second argument is the operand of the function.
ST Language
Q := RIGHT (IN, NBC);
FBD Language
FFLD Language
(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
See also