Real Time Clock Management Functions
The following functions read the real time clock of the target system:
The following functions format the current date/time to a string:
| DAY_TIME | With predefined format |
| DTFORMAT | With custom format |
The following functions are used for triggering operations:
| DTAt | Pulse |
| DTEvery | Pulse signal with long period |
-
-
The real-time clock may not be available on all controller hardware models. Please consult the controller hardware specifications for real-time clock availability.
DAY_TIME: get current date or time
Q := DAY_TIME (SEL);
SEL : DINT specifies
the wished information (see below)
Q : STRING wished information formatted on a
string
Possible values of SEL input
1 current time - format: 'HH:MM:SS'
2 day of the week
0 (default) current date - format: 'YYYY/MM/DD'
DTCURDATE: get current date stamp
Q := DTCurDate ();
Q : DINT numerical stamp representing the current date
DTCURTIME: get current time stamp
Q := DTCurTime ();
Q : DINT numerical stamp representing the current time of the day
DTYEAR: extract the year from a date stamp
Q := DTYear (iDate);
IDATE : DINT numerical
stamp representing a date. This is output of DTCURDATE.
Q : DINT year of the date (ex: 2004)
DTMONTH: extract the month from a date stamp
Q := DTMonth (iDate);
IDATE : DINT numerical
stamp representing a date. This is output of DTCURDATE.
Q : DINT month of the date (1..12)
DTDAY: extract the day of the month from a date stamp
Q := DTDay (iDate);
IDATE : DINT numerical
stamp representing a date. This is output of DTCURDATE.
Q : DINT day of the month of the date (1..31)
DTHOUR: extract the hours from a time stamp
Q := DTHour (iTime);
ITIME : DINT numerical
stamp representing a time. This is output of DTCURDATE.
Q : DINT Hours of the time (0..23)
DTMIN: extract the minutes from a time stamp
Q := DTMin (iTime);
ITIME : DINT numerical
stamp representing a time. This is output of DTCURDATE.
Q : DINT Minutes of the time (0..59)
DTSEC: extract the seconds from a time stamp
Q := DTSec (iTime);
ITIME : DINT numerical
stamp representing a time. This is output of DTCURDATE.
Q : DINT Seconds of the time (0..59)
DTMS: extract the milliseconds from a time stamp
Q := DTMs (iTime);
ITIME : DINT numerical
stamp representing a time. This is output of DTCURDATE.
Q : DINT Milliseconds of the time (0..999)