Sig_Gen
A function block groups an algorithm and a set of private data. It has inputs and outputs. - Generator of pseudo-analogical Signal
Inputs
RUN : BOOL Enabling command
PERIOD : TIME Signal period
MAXIMUM : DINT Maximum growth during the signal period
Outputs
This FB generates signals of the four following types:
- PULSE: blinking at each period
- UP : growing according max * period
- END : pulse after max * period
- SINE : sine curve
FFLD Language