| BZ-10575 |
PipeNetwork Trigger block does not support a non-modulo input. |
| BZ-10458 |
Variable Creation Wizard don't show the mapping. |
| BZ-10451 |
Cannot start application with direct connection. |
| BZ-10419 |
Drag 'n' drop variable from instance to watch window does not display the value. |
| BZ-10275 |
PxMM controller bus time not synchronized with DC master time. |
| BZ-9975 |
KAS crashes in the Workbench Performance Servo Tuner Window. |
| BZ-9928 |
ESI file list is not updated when good and bad ESI files are added at the same time. |
| BZ-9835 |
Non-ASCII characters in projects not handled properly in the KAS IDE. |
| BZ-9834 |
Import/export from/to non-ascii file names does not work correctly. |
| BZ-9496 |
AKD-N firmware download fails if 4x drives are selected. |
| BZ-9359 |
PDO objects not defined in the object dictionary (or 24bit size) will not work properly with MLSmpXxxxx(...) functions. |
| BZ-8659 |
move blending with . If the blending move is commanded with an unreachable velocity, the move may abruptly decelerate to the final position within one sample, exceeding the specified deceleration rate. |
| BZ-8654 |
E21 when KAS IDE running O-Scope is disconnected. |
| BZ-8645 |
Adding ESI File After Scanning Results in No Selected PDOs. |
| BZ-8644 |
PLCopen S-Curve move may not reach target with small . |
| BZ-8643 |
scan fails after a AKD drive firmware download failure with a wrong EtherCAT topology. |
| BZ-8636 |
Recovered projects don’t recover imported libraries (.kal files). |
| BZ-8608 |
KAS IDE views do not scale if Windows text scaling is > 100%. |
| BZ-8605 |
MLInitTrig does not configure the AKD Capture engine correctly for a negative edge trigger. |
| BZ-8588 |
ECAT network restore fails to recover from drive FW download failure. |
| BZ-8508 |
PDOs need padding to meet byte boundary requirement. The IDE PDO Editor does not automatically pad PDOs on non-byte boundaries. The problem can be avoided by manually adding dummy objects to pad the PDO size to line-up on byte boundaries. For more details, see the article on KDN. |
| BZ-8504 |
KL3314 Operation. Temperature values are not calibrated properly to the thermocouple. To work-around the problem, use ECATWriteData to setup the control word (16xE0) and send value (16x2006) to Register R32 and a second ECATWriteData to write zero (0) to the control word to set up the continual output of the temperature. |
| BZ-8482 |
renumber address does not work with String variables. In the Editor Modbus configurator, if you right click input registers and choose the renumber address option, it will make the addresses overlap. |
| BZ-8212 |
Modified cam file is not downloaded when forcing an Online Change. |
| BZ-8138 |
WebBrowser component not working for TxB panels. |
| BZ-8132 |
K-Bus slices analog inputs Offset parameter does not work. |
| BZ-7985 |
IDE disconnects from the controller after several days. |
| BZ-7759 |
Breakpoint with For(…) loop, increases VM load significantly. |
| BZ-7728 |
IDE animation with non-matching project versions. |
| BZ-6240 |
IDE always reports the project has been modified. |