| BZ-8242 |
Missed cycles while doing file operations. |
| BZ-8633 |
When a crash report fails due to error (ex: timeout, connection failure, …) report is lost. User cannot resend. |
| BZ-9832 |
Cannot add libraries (.KAL files) with non-ASCII file names. |
| BZ-9848 |
KAS broken if Windows user name contains non-ASCII characters. |
| BZ-10453 |
ESI CheckRevisionNo Algorithms are not Implemented. Warning! This change causes an incompatibility with previous KAS IDE versions. |
| BZ-10456 |
KAS IDE WorkBench freeze, partial tree/no views, or crash occur with heavy loading. |
| BZ-10485 |
Duplicate CoE InitCmds for AKD2G Safety Models with Modules |
| BZ-10498 |
Adding more than one axis to axis group from project tree fails. |
| BZ-10509 |
MOD/MODR/MODLR with zero input or negative base. |
| BZ-10526 |
KAS IDE will crash at Motion Engine Selector after import PipeNetwork. |
| BZ-10538 |
MC_CamResumePos(...) output value incorrect with relative position camming. |
| BZ-10546 |
axis user units cannot be set to a specific value. |
| BZ-10550 |
Online Config Mode Fault with large networks. |
| BZ-10568 |
KAS IDE Editor view fails to open properly. |
| BZ-10577 |
Actual position jitter via EtherCAT. |
| BZ-10581 |
KAS IDE O-Scope w/ large time base blocks the forcing variable pop-up. |
| BZ-10593 |
PDO size in the KAS IDE FSoE/PDO connections tab view does not include padding. |
| BZ-10598 |
KAS IDE WorkBench unresponsive with slow and Control Panel. |
| BZ-10599 |
MLAxisReAlign doesn't work if DeltaPos input is greater than the modulo. |