Download AKD PDMM Drive Firmware
Component | Title | Download |
---|---|---|
800MHz AKD PDMM Drive FW | AKD PDMM Servo Drive![]() |
![]() |
1.2GHz AKD PDMM Drive FW | AKD PDMM Servo Drive Firmware (AKD-M-M1EC-[firmware version]) | ![]() |
To upgrade AKD PDMM drive Firmware with KAS IDE"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger, continue from the previous procedure as follows:
- In the toolbar, deactivate the Online Configuration Mode.
- Select the drives requiring the same firmware version to be updated .
Please note that the firmware download is limited to 16 drives at a time.
- Click Upgrade Firmware button.
Give careful attention to any warning dialog that appears at this point. These warnings usually include important information about preventing damage to the drives.
- Browse to select the new AKD/AKD2G firmware file.
- Click Open to start the updating procedure.