MLAxisMoveVel![This function or function block supports Pipe Network motion Pipe Network motion icon](../../Resources/Images/Icon_PipeNetwork.png)
Description
Jog at the specified speed. Returns TRUE if the function succeeded.
Arguments
Input
ID |
Description |
ID Name of the Axis block. |
Data type |
DINT |
|
Range |
— |
|
Unit |
N/A |
|
Default |
— |
|
Speed |
Description |
Sets the Axis Speed. |
Data type |
LREAL |
|
Range |
— |
|
Unit |
User unit/sec |
|
Default |
— |
Output
Default (.Q) |
Description |
Returns true when function successfully executes, after the motion has reached jog speed. See more details here. |
Data type |
BOOL |
|
Unit |
N/A |
Related Functions
Previous Function Name
Example
See Usage Example of Axis Functions for additional examples.
Structured Text
MLAxisMoveVel(PipeNetwork.Axis1, 500 ) ;
|
Ladder Diagram
Function Block Diagram