MLAxisRstFastIn![This function or function block supports Pipe Network motion Pipe Network motion icon](../../Resources/Images/Icon_PipeNetwork.png)
Description
Write in the LatchThe control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT bus cycle. The status word is used to return the drive's latch status Control Word to reset the Fast Input
The inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action.
Arguments
Input
AxisID |
Description |
ID Name of the Axis block. |
Data type |
DINT |
|
Range |
— |
|
Unit |
N/A |
|
Default |
— |
|
InputID |
Description |
ID name of the Fast input to be reset on an axis, (ie IN1 and IN2 on S300 0 = Touch Probe 1 / Capture Engine 0 1 = Touch Probe 2 / Capture Engine 1 Range is [0,1] |
Data type |
DINT |
|
Range |
— |
|
Unit |
N/A |
|
Default |
— |
Output
Default (.Q) |
Description |
Returns true when function successfully executes. See more details here. |
Data type |
BOOL |
|
Unit |
N/A |
Related Functions
Example
Structured Text
MLAxisRstFastIn(PipeNetwork.Axis1, 0 ) ;
|
Ladder Diagram
Function Block Diagram