FunctionMLAxisWritePosPipe Network motion icon

Description

Used to set a position offset at the Axis when the Pipe Network:

  • Pipe Position and Pipe Offset are set to zero
  • Generator Position is set to equal to Zero Position
  • Then Reference Position equals Pipe Position + Generator Position

Arguments

Input

ID

Description

ID Name of the Axis block.

 

Data type

DINT

 

Range

—

 

Unit

N/A

 

Default

—

Position

Description

Position offset.

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

Default (.Q)

Description

Returns true when function successfully executes.

See more details here.

 

Data type

BOOL

 

Unit

N/A

Previous Function Name

MLAxisSetZero

Example

Structured Text

 MLAxisWritePos( PipeNetwork.Axis1, 0) ;

Ladder Diagram

MLAxisWritePos: LD example

Function Block Diagram

MLAxisWritePos: FBD example

Go back to the top of the page [Top]