MC_GrpStop![This function or function block supports PLCopen motion PLCopen motion icon](../../Resources/Images/Icon_PLCopen.png)
![This function or function block supports Pipe Network motion Pipe Network motion icon](../../Resources/Images/Icon_PipeNetwork.png)
Description
MC_GrpStop performs a controlled motion stop of all axes in the group. When the path velocity reaches zero any queued moves are flushed from the buffer and the Done output is set. When both the Done output is true and the application has cleared the Execute input the state transitions to GroupStandby. MC_GrpStop can not be aborted.
-
-
MC_GrpStop does NOT prevent a single axis from executing nor does it prevent other Coordinated Motion moves from executing once MC_GrpStop has completed.
-
- This function block starts a motion-related action and therefore stores data for calculations and error checking. Please see Calling Function Blocks Multiple Times in the Same Cycle if you are using a dual-core controller.
Related Functions
MC_GrpHalt, MC_ErrorDescription
Coordinated Motion, the top-level topic for Coordinated Motion.
Arguments
For more details on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules.
Input
Execute | Description | On the rising edge![]() |
Data type | BOOL | |
Range | 0, 1 | |
Unit | N/A | |
Default | — | |
AxesGroup | Description | The axes group in which the axes will be stopped. |
Data type | AXES_GROUP_REF | |
Range | N/A | |
Unit | N/A | |
Default | — | |
Deceleration | Description | The path deceleration rate for all of the axes in the group |
Data type | LREAL | |
Range |
0 < Deceleration See Limitations on Acceleration and Jerk for more information. |
|
Unit | N/A | |
Default | — | |
Jerk | Description | Not supported |
Data type | LREAL | |
Range |
0 ≤ Jerk See Limitations on Acceleration and Jerk for more information. |
|
Unit | N/A | |
Default | — |
Output
Done | Description | If True, then the command completed successfully. |
Data type | BOOL | |
Busy | Description | TRUE from the moment the EXECUTE input is TRUE until the stop is complete. |
Data type | BOOL | |
Active | Description | If True, then the stop is still executing. |
Data type | BOOL | |
Error | Description | If True, an error has occurred. |
Data type | BOOL | |
ErrorID | Description | Indicates the error identifier if Error output is set to TRUE. See table in PLCopen Function Block ErrorID Output. |
Data type | INT |
Example
Structured Text
Inst_MC_GrpStop ( EnableStop, Group1_Ref, Deceleration, Jerk );
IL
BEGIN_IL"Instruction list" This is a low-level language and resembles assembly CAL Inst_MC_GrpStop ( EnableStop, Group1_Ref, Deceleration, Jerk ) END_IL
FBD
FFLD