Function BlockFileRenamePLCopen motion icon

Description

This function block renames a file.

Figure 8-210: The FileRename Function Block

Related Functions

FileCopy, FileDelete, FileExists, FileSize

See also: File Management

Arguments

Input

Execute Description On the rising edgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge request to rename a file
  Data Type BOOL
  Range 0, 1
  Unit N/A
  Default —
Path Description The path to the file to be renamed
  Data Type STRING
  Range N/A
  Unit N/A
  Default —
NewName Description The new name of the file
  Data Type STRING
  Range N/A
  Unit user units
  Default —

Output

Done Description If TRUE, then the command completed successfully
  Data Type BOOL
Error Description If TRUE, an error has occurred
  Data Type BOOL
ErrorID Description Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output
  Data Type DINT

Example

Structured Text

(* FileRename example *)
CASE StepCounter OF
0:
  Inst_FileRename(TRUE, 'Original.txt', 'Renamed.txt');
  StepCounter := StepCounter + 1;
1:
  Inst_FileRename(TRUE, 'Original.txt', 'Renamed.txt');
  IF Inst_FileRename.Done THEN
     Inst_FileRename(FALSE, '', '');
     StepCounter := StepCounter + 1;
  END_IF;
END_CASE;