File Path Conventions
Depending upon the system used, paths to file locations may be defined as either absolute (C://dir1/file1
) or relative paths (/dir1/file1
). Not all systems handle all options, and the paths will vary depending upon the system.
System | Absolute Paths | Relative Paths | Handling of Directories |
---|---|---|---|
AKD PDMM or PCMM |
![]() |
![]() |
There is no support for creating directories on the controller. Any path provided to the function blocks, file1 for example, will be appended with the default userdata folder which is:/mount/flash/userdata |
Simulator |
![]() |
![]() |
When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Simulator/Application/userdata |
PAC |
![]() |
![]() |
When a relative path is provided to the function blocks, the path is appended with the default userdata folder, which is:<User Directory>/Kollmorgen/Kollmorgen Automation Suite/Sinope Runtime/Application/userdata |
See Also: