FunctionMC_InitAxisPLCopen motion icon

Description

MC_InitAxis initializes a PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML Servo Axis' data. A call to this function is automatically generated when the application is compiled, based on the data entered in the PLCopen Axis Data dialog.

MC_InitAxis

Figure 8-123: MC_InitAxis

Arguments

For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules

Input

En

Description

Request to initialize a PLCopen servo axis

 

Data type

BOOL

 

Range

0, 1

 

Unit

N/A

 

Default

—

AxisNumber

Description

Servo axis number

 

Data type

UINT

 

Range

[1,256]

 

Unit

none

 

Default

—

VelocityLimit

Description

Reserved for future use

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec

 

Default

—

LowerLimit

Description

Reserved for future use

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

UpperLimit

Description

Reserved for future use

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

LimitControl

Description

Reserved for future use

 

Data type

UINT

 

Range

[0,2]

 

Unit

N/A

 

Default

—

PosErrorLimit

Description

Position error limit – when the Position Error

(command position – actual position) exceeds this value, an E-stop is generated

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

InPositionBand

Description

In-position bandwidthClosedIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz – when the axis actual position is within this distance from its programmed endpoint, the axis is considered “in position”

 

Data type

LREAL

 

Range

—

 

Unit

User unit

 

Default

—

Output

OK

Description

Indicates the initialization is complete

See more details here.

 

Data type

BOOL

Example

Structured Text

(* MC_InitAxis STClosed"Structured text"
A high-level language that is block structured and syntactically resembles Pascal example *)
AxisNumber1 := 1;
VelocityLimit1 := 10000; (*User unit/second*)
LowerPosLimit1 := 0;
UpperPosLimit1 := 0;
LimitControl1 := 0; (* Ignore lower and upper pos limit*)
PosErrorLimit1 := 10; (*User unit*)
InPosBand1 := 0;
MC_InitAxis(AxisNumber1, VelocityLimit1, LowerPosLimit1, UpperPosLimit1, LimitControl1, PosErrorLimit1, InPosBand1);

Function Block Diagram

Ladder Diagram

MC_InitAxis: LD example

Go back to the top of the page [Top]