MLFB_HomeUsingCurrentPosition![This function or function block supports Pipe Network motion Pipe Network motion icon](../Resources/Images/Icon_PipeNetwork.png)
Description
Using the current position is the most basic homing method. This method simply uses the current position of the motor as the home point reference.
You can use this parameter to set the value of the home position other then zero. This allows you to offset your home reference away from zero.
Arguments
Input
ibExecute |
Description |
Start homing, edge-triggered |
Data type |
BOOL |
iAxisID |
Description |
ID of Axis block of Pipe Network |
Data type |
DINT |
iPosition |
Description |
Reference position |
Data type |
LREAL |
Output
obDone |
Description |
Done bit |
Data type |
BOOL |
obActive |
Description |
Active bit |
Data type |
BOOL |
obError |
Description |
Error bit |
Data type |
BOOL |
oErrorID |
Description |
Error identifier, see list here
|
||||||||||||
Data type |
DINT |
Example
ST
//No movement, set current axis position to position input in this case zero
Inst_MLFB_HomeUsingCurrenctPosition( StartHomeRoutine, PipeNetwork.AXIS1, 0 );
HomeDone := Inst_MLFB_HomeUsingCurrenctPosition.obDone;
Function Block Diagram
FFLD