MLGearReadRatio![This function or function block supports Pipe Network motion Pipe Network motion icon](../Resources/Images/Icon_PipeNetwork.png)
Description
Returns the Ratio value of a selected Gear Block from the Pipe Network. The output of a Gear Block = Input value * Ratio + Offset
Arguments
Input
BlockID |
Description |
ID number of an initialized Gear Pipe Block |
Data type |
DINT |
|
Range |
[-2147483648, 2147483648] |
|
Unit |
N/A |
|
Default |
— |
Output
Ratio |
Description |
The Ratio value currently assigned to the selected Gear Pipe Block |
Data type |
LREAL |
|
Unit |
N/A |
Related Functions
Example
Structured Text
//Find the Ratio value of Gear1 Pipe Block
Gear1Ratio := MLGearReadRatio(PipeNetwork.GEAR1);
Ladder Diagram
Function Block Diagram