MLGearWriteOff![This function or function block supports Pipe Network motion Pipe Network motion icon](../Resources/Images/Icon_PipeNetwork.png)
Description
Sets the Offset value of a selected Gear Pipe Block.
The output of a Gear Block = Input value * Ratio + Offset
-
-
Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8)
Arguments
Input
BlockID |
Description |
ID number of an initialized Gear Pipe Block |
Data type |
DINT |
|
Range |
[-2147483648, 2147483648] |
|
Unit |
N/A |
|
Default |
— |
|
Offset |
Description |
New Offset value to be assigned to selected Gear Pipe Block. Values lower then 1.0 can be entered, but require a leading zero (for example 0.8 instead of .8) |
Data type |
LREAL |
|
Range |
— |
|
Unit |
User unit |
|
Default |
— |
Output
Default (.Q) |
Description |
Returns TRUE if Offset value is changed in the selected Gear Pipe Block See more details here. |
Data type |
BOOL |
|
Unit |
N/A |
Return Type
BOOL
Related Functions
Example
Structured Text
//Set the Offset value of Gear1 Pipe Block to 5 User Units MLGearWriteOff(PipeNetwork.GEAR1, 5.0);
|
Ladder Diagram
Function Block Diagram