MLPhaReadPhase![This function or function block supports Pipe Network motion Pipe Network motion icon](../Resources/Images/Icon_PipeNetwork.png)
Description
Get the phase value of a phaser block.
Arguments
Input
BlockID |
Description |
ID Name of a Phaser function block in the Pipe Network |
Data type |
DINT |
|
Range |
[-2147483648, 2147483648] |
|
Unit |
N/A |
|
Default |
— |
Output
Phase |
Data type |
LREAL |
Example
Structured Text
PresentPhase := MLPhaReadPhase( PipeNetwork.PhaseAdjust );
|
Ladder Diagram
Function Block Diagram