Motion Library - Pipe Network

Name

Description

Return type

MLPipeAct

Activates a pipe

BOOL

MLPipeAddBlock

Adds a Pipe Block to a pipe

BOOL

MLPipeCreate

Creates a new pipe object

None

MLPipeDeact

Deactivates a pipe

BOOL

FunctionMLPipeActPipe Network motion icon

Description

Activates a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block. The first ends with the first converter, and has a Gear Pipe Block to transform the input values from the Master. The second pipe ends with the second converter, and has a CAM Pipe Block to modify the input values from the Master.

Once a Pipe is activated then history on the values in the Pipe's Blocks are saved and updated each program cycle. A Converter object connected to a destination Axis object cannot send updated position values unless its Pipe is activated.

MLPipeAct

Figure 8-62: MLPipeAct


  • All Pipes in the Pipe Network can be activated at once with the command PipeNetwork(MLPN_ACTIVATE). This calls automatically generated code with MLPipeAct commands for each Pipe object. Therefore, in a multi-pipe program only one command can be used to activate Pipes instead of writing code for each Pipe separately.

Arguments

Input

PipeID

Description

ID number of a created Pipe object

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe is activated

See more details here.

 

Data type

BOOL

 

Unit

N/A

Return Type

BOOL

Related Functions

MLPipeDeact

MLCNVConnect

PipeNetwork(MLPN_ACTIVATE)

MLPipeAddBlock

Example

Structured Text

 

//Activate a Pipe

MLPipeAct( PipeAXIS1 );

 

Ladder Diagram

MLPipeAct: LD example

 

Function Block Diagram

MLPipeAct: FBD example

Go back to the top of the page [Top]

FunctionMLPipeAddBlockPipe Network motion icon

Description

Add a Pipe Block to a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between.

The figure below shows two Pipes, both with the same Master Input Pipe Block. If a user were to create the Pipe 1 below without using the Graphical Engine, they would use the following commands once a Pipe and the Pipe Blocks have been created.

MLPipeAddBlock( PipeAXIS1, MASTER);

MLPipeAddBlock( PipeAXIS1, MyGear);

MLPipeAddBlock( PipeAXIS1, CNV1);

MLPipeAddBlock

Figure 8-63: MLPipeAddBlock


  • All Blocks in the Pipe Network are added to a Pipe automatically. Code with MLPipeAddBlock commands are automatically generated and called in a program with PipeNetwork(MLPN_CREATE_OBJECTS). Therefore, when using the Pipe Network graphical engine to create Pipe Blocks the user does not have to manually add MLPipeAddBlock commands to the Project.

Arguments

Input

PipeID

Description

ID number of a created Pipe

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

BlockID

Description

ID number of a created Pipe object to add to the selected Pipe

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe Block is added to the Pipe

See more details here.

 

Data type

BOOL

 

Unit

N/A

Return Type

BOOL

Related Functions

PipeNetwork(MLPN_CREATE_OBJECTS)

MLPipeAct

MLPipeCreate

MLPipeDeact

Example

Structured Text

 

//Add a block to a pipe

MLPipeAddBlock( PipeAXIS1, MyGear );

 

Ladder Diagram

MLPipeAddBlock: LD example

 

Function Block Diagram

MLPipeAddBlock: FBD example

Go back to the top of the page [Top]

FunctionMLPipeCreatePipe Network motion icon

Description

Create a new pipe object. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block.


  • Pipes are normally created in the Pipe Network using the graphical engine. Then you do not have to add MLPipeCreate function blocks to their programs. Pipes are created graphically, and the code with MLPipeCreate commands are automatically generated and called in a program with PipeNetwork(MLPN_CREATE_OBJECTS).

Arguments

Input

Name

Description

Desired name for the newly created Pipe

 

Data type

String

 

Range

—

 

Unit

N/A

 

Default

—

Output

ID

Description

Assigned ID number of the created Pipe

 

Data type

DINT

 

Unit

N/A

 

Default

—

Related Functions

PipeNetwork(MLPN_CREATE_OBJECTS)

MLPipeAddBlock

MLPipeAct

MLPipeDeact

Example

Structured Text

 

//Create a new pipe

PipeAXIS1 := MLPipeCreate( 'PipeAXIS1' );

 

 

Ladder Diagram

MLPipeCreate: LD example

 

Function Block Diagram

MLPipeCreate: FBD example

Go back to the top of the page [Top]

FunctionMLPipeDeactPipe Network motion icon

Description

Deactivates a pipe. A Pipe contains an Input Pipe Block (Master, PMP, or Sampler), a Converter Output Pipe Block, and any Transformation Pipe Block that can be in between. The figure below shows two Pipes, both with the same Master Input Pipe Block. The first ends with the first converter, and has a Gear Pipe Block to transform the input values from the Master. The second pipe ends with the second converter, and has a CAM Pipe Block to modify the input values from the Master.

Once a Pipe is activated then history on the values in the Pipe's Blocks are lost and no longer updated. A Converter object connected to a destination Axis object cannot send updated position values once its Pipe is deactivated.

MLPipeDeact

Figure 8-64: MLPipeDeact


  • All Pipes in the Pipe Network can be deactivated at once with the command PipeNetwork(MLPN_DEACTIVATE). This calls automatically generated code with MLPipeDeact commands for each Pipe object. Therefore, in a multi-pipe program only one command can be used to deactivate Pipes instead of writing code for each Pipe separately.

Arguments

Input

PipeID

Description

ID number of a created Pipe object

 

Data type

DINT

 

Range

[-2147483648, 2147483648]

 

Unit

N/A

 

Default

—

Output

Default (.Q)

Description

Returns TRUE if the Pipe is deactivated

See more details here.

 

Data type

BOOL

 

Unit

N/A

Return Type

BOOL

Related Functions

MLPipeAct

MLCNVDisconnect

PipeNetwork(MLPN_DEACTIVATE)

MLPipeAddBlock

Example

Structured Text

 

//Deactivate a Pipe

MLPipeDeact( PipeAXIS1 );

 

Ladder Diagram

MLPipeDeact: LD example

Function Block Diagram

MLPipeDeact: FBD example

Go back to the top of the page [Top]