CANopen Status Word
The status machine for the control word corresponds to the CANopen status machine.
The status word is only updated and written by the drive in Safe-Op and Operational states.
Bits definition of the status word
| Bit | Name |
|
0 |
Ready to switch on |
|
1 |
Switched on |
|
2 |
Operation enable |
|
3 |
Fault |
|
4 |
Voltage enabled |
|
5 |
Quick stop |
|
6 |
Switch on disabled |
|
7 |
Warning |
|
8 |
Manufacturer-specific (reserved) |
|
9 |
Remote (always 1) |
|
10 |
Target reached |
|
11 |
Internal limit active |
|
12 |
Operation mode specific (reserved) |
|
13 |
Operation mode specific (reserved) |
|
14 |
Manufacturer-specific (reserved) |
|
15 |
Manufacturer-specific (reserved) |
Table 6-9: Bit Assignment in Status Word
The bit combinations coding the following states are listed in the table below.
| Status word MSB |
State |
|
xxxx xxxx x0xx 0000 |
Not ready to switch on |
|
xxxx xxxx x1xx 0000 |
Switch on disabled |
|
xxxx xxxx x01x 0001 |
Ready to switch on |
|
xxxx xxxx x01x 0011 |
Switched on |
|
xxxx xxxx x01x 0111 |
Operation enabled |
|
xxxx xxxx x00x 0111 |
Quick stop active |
|
xxxx xxxx x0xx 1111 |
Fault reaction active |
|
xxxx xxxx x0xx 1000 |
Fault |
Bits marked by an X are irrelevant
For more details about the Status Word in the AKD™ CANopen Communication, click here.