Create KVB Project
KVB projects are managed in the Project Explorer and can be created as follows:
- In the Project Explorer, right-click on the System item to open the contextual menu
- Select the Add HMI
"Human-machine interfaces "
Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response device command - Select the device name within the list and Click OK

-
-
The content will vary depending upon what version of KVB is installed on your system. If you have KVB 1.1 installed you may open projects that have a KVB 2.1 panel, but you will not be able to open the panel in KVB.
- Right-click on the newly created item and select the Rename command to change its name
- Right-click and select the Add KVB Project command
Figure 5-26: Select an AKI to add.
-
-
Note that this command is disabled when a KVB panel is already created for the current HMI device