How to Plug PLC Variables
- In the Variable Dictionary, right-click on the variable lastMachineSpeed to open its menu
- Choose the command Plug on channel

- Set Channel to 2(because channel 1 is already plugged)

Figure 5-65: Plugging a PLC Variable
You can start the Softscope now to see traces, as shown in the following figure:
Figure 5-67: Traces Displayed with Soft Oscilloscope
-
-
Easy probe plugging is assured since you do not need to unplug a probe from a channel before plugging a new probe into the same channel.