Cam Profile Editor
About the Cam Profile Editor
The cam profile editor enables you to create and/or modify a profile definition that describes the position evolution of the cam. This evolution is displayed in a 2D graphical format.
You can add, delete, or modify cam elements which consist of points and lines. Based on those elements and some constraints, the KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger calculates a complete cam shape. See Cam Profile Segment Overview for more information on the segment types.
Master/Input (X-Axis) and Slave/Output (Y-axis) coordinates can be specified to define the position.
In addition to the position, it is also possible to visualize the velocity, acceleration, and jerk
In physics, jerk is the rate of change of acceleration; more precisely, the derivative of acceleration with respect to time diagrams.
Windows Overview
Figure 7-10: Cam Profile Editor Main Window
The cam profile editor contains four distinct parts separated by splitters:
- The cam table (see call out
) displays each element and allows editing of the cam. - The Graphical Area for the cam profile

The upper graph displays a graphical representation of the cam elements - The Curve Selection and Color Table
allows you to select which plots (velocity, acceleration and jerk) are displayed - The Graphical Area for Curves

The lower graph displays a graphical representation of the velocity, acceleration and jerk plots
-
-
Undo (Ctrl+Z) and Redo (Ctrl+Y) operations are available for any changes you make to the cam profile.
Splitters allow you to resize each part.
-
-
The tables and the graphs are separated by a vertical splitter so that you can completely hide the tables to increase the graphical area.
For more information on cam profiles see Adding Cam Profiles and Profiles.