Tools Menu
|
Command |
Description |
|
Oscilloscope |
Show the soft oscilloscope |
|
Compile (Ctrl + B) |
Compile the whole project |
| Compile & Download (Ctrl + F7) | Compile the whole project and download it to the controller. |
| User Options |
Open the User Options dialog box. |
Table 5-5: Tools Menu Commands
User Options
AKD GUI Scope Settings
The check box found in this dialog enables/disables the “Load at startup” option in the AKD GUI
"Graphical User Interface"
A GUI is a type of user interface which allows people to interact with a computer and computer-controlled devices Scope “settings” tab.![]()
AutoSave Recovery File Settings
This option Enables / Disables automatically saving project recovery files at a specified interval. Once set, this applies to all further project recovery files for the user. The stopwatch icon in the bottom right corner of the KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger indicates whether AutoSave Recovery Files is active
or disabled
. See How does file recovery work? for information about recovery files.