Online Change Toolbar

Each icon provided in this toolbox has a brief explanation provided below to explain the functionality.

Icon

Description

When Online Change has been activated in the PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events options; the new code is loaded even if the application is running.
See also the Warning in How to Activate Online Change

Revert your changes done after an Online Change, and go back to the previous application

Table 5-11: Debug Toolbar Icons