ACTION#.SOURCE
Description
This keyword defines the input source for an action.
| Value | Description |
|---|---|
| 0 | No source |
| 1 | Mains ready |
| 2 | Digital Input |
| 3 | Digital Dio (Bidirectional) |
| 4 | Velocity Feedback |
| 5 | Axis Faulted |
| 6 | Home Complete |
| 7 | Motion Task in Position |
| 8 | Controlled Stop Active |
| 9 | Software Limit |
| 10 | Move Complete |
| 11 | Position Error, Absolute |
| 12 | Axis Enabled |
| 13 | Analog Input |
| 14 | Current Command |
| 15 | Velocity Error |
| 16 | Velocity Command |
| 17 | Position Feedback |
| 18 | Axis Disable Immediately |
| 19 | Brake State |
| 20 | Ready to Operate (RTO/BTB) |
| 21 | Compare Digital Inputs |
| 22 | Feedback Fault |
| 23 | User Variable |
| 25 | Current Feedback |
| 200 | Safe Input |
| 201 | Safe Dual Input |
| 202 | Safe Output |
| 203 | Safe Dual Output |
| 204 | STO active |
| 205 | SS1 active |
| 206 | SS2 active |
| 207 | SOS active |
| 208 | SBC active |
| 209 | SLS active |
| 210 | SSM active |
| 211 | SSR active |
| 212 | SDI_n active |
| 213 | SDI_p active |
| 214 | SLA active |
| 215 | SAR active |
| 216 | SLI active |
| 217 | SLP active |
| 218 | SCA active |
21 - Compare Digital Outputs
Some actions need to be triggered based on the state of multiple digital inputs. For such cases, the Compare Digital Inputs action source provides a mechanism for specifying a combination of digital input values.
A 32-bit word containing the states of all DIN pins (DIN.STATES) and bidirectional digital IO pins (DIO.STATES) is updated prior to running the action table rows. DINs are assigned bits 0-19, and DIOs are assigned bits 20-31.
To set up an action to run based on a digital input combination, set ACTION#.SOURCE to 21 (Compare Digital Inputs). ACTION#.SOURCEID is unused, and ACTION#.SOURCEPARAM defines a mask corresponding to the pins you wish to check. For example, to check DIN2, DIN5, and DIO3, set ACTION#.SOURCEPARAM to 4194322 (0x00400012).
Set ACTION#.CONDITIONVALUE to the specific value of the digital input combination you want to match. Continuing the example, to match the combination DIN2 = 1, DIN5 = 0, and DIO3 = 1, set ACTION#.CONDITIONVALUE to 4194306 (0x00400002).
When ACTION#.CONDITION is 2 (Follows) the comparison is continuously true if the digital input match is successful. When ACTION#.CONDITION is 1 (Inverts) the comparison is true if one or more of the digital inputs does not match its specified value. When ACTION#.CONDITION is 5 (Rising Edge
A rising edge is the transition of a digital signal from low to high. It is also called positive edge) the comparison triggers the action task on the first sample where the digital input matches. When ACTION#.CONDITION is 6 (Falling Edge) the comparison triggers the task on the first sample where one or more digital inputs fails to match.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 20 |
|
Default Value |
0 (no source) |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.