AIN#.VALUE
Description
AIN#.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
Examples
Code
--> AIN1.VALUE 1.420 V
Context
For more information see Analog Input.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | V |
Range | -12.5V to +12.5V |
Default Value | N/A |
Data Type | Float |
See Also | |
Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AIN1.VALUE | 0x3780 | 0x1 | INT | 1000:1 | - | RO | True |
AIN2.VALUE | 0x3781 | 0x1 | INT | 1000:1 | - | RO | True |