AXIS#.MOTOR.RTYPE
Description
This parameter defines the type of thermal resistor inside the motor to measure motor temperature. The following resistor types are supported:
AXIS#.MOTOR.RTYPE | Thermal Resistor Type |
---|---|
0 | PTC |
1 | NTC |
2 | KTY83-110 |
3 | KTY84-130 |
4 | PTC + KTY83-110 |
5 | Thermal switch |
6 | PTC + PT1000 |
7 | PTC + PTC |
8 | PT1000 |
127 | No sensor![]() |
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1 and motor memory version is 0.3 or greater.
See Motor Temperature.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 8, 127 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.MOTOR.RTYPE | 0x500B | 0x19 | USINT | - | - | RW | False |
AXIS2.MOTOR.RTYPE | 0x510B | 0x19 | USINT | - | - | RW | False |