AXIS#.SM.ACC
Description
Sets the acceleration ramp for service motion.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM See Acceleration Units for details. |
Range |
Depends on units. See Acceleration Units for details. |
Default Value |
30,000 rpm/s Depends on units. See Acceleration Units for details. |
Data Type |
Float |
See Also | |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported